Changing the network settings

Make sure that your network configuration is valid. If your configuration is invalid, you might lose network access to the device. In this case, a reset of the network settings is necessary. All ethernet ports in u-OS are independent network interfaces which do not provide switch functionality between each other.

Only enter IP addresses that are outside the Docker network. IP addresses within the Docker network can cause problems with apps in u-OS. In the delivery state, the range of the Docker network is located at 172.16.0.0/12. If you have changed the Docker network range, enter IP addresses outside the range you have set.

Enter a maximum of 3 DNS servers for all network interfaces together. If you enter more, problems might occur with the name resolution.

For an overview of the default IP addresses, see Overview of the communication interfaces.

When configuring the network settings, you can set static or DHCP configuration.
- static: one manually configured static IP address
- DHCP: the network interface can have two IP addresses at the same time. One IP address assigned by the DHCP server and one IP address manually configured.
- You have opened the u-OS Control Center.
- Click Network & internet.
- Click Edit.
- Choose the tab of the Ethernet network whose settings you want to change.
- Choose between static and dynamic (DHCP) mode for the IP configuration.
- Change the following data:
- IP address
- Subnet mask
- Default gateway (optional)
- DNS servers (optional)
- Click Apply.