ResMa 3.7.0¶
Release date: 2024-03-26
Service compatibility¶
This ResMa version is compatible with
Recipe Service v1.3.3
Import Service v1.1.0
Regression Service v1.0.0
Operating system compatibility¶
Windows 10 Pro
Windows 10 Enterprise
Windows 10 IoT Enterprise
Windows Server 2016
Windows Server 2019
Windows Server 2022
Features¶
19354: Testing of derived variables during generation/modification
54789: Add logs on the web page
74423: Logs from DirectConntect are saved now
75091: Log of “HiveMQService” und “IIoTCommunicationService” get saved
80365: Reset-Buttons are deleted in the PageTools
80372: Edit mode will now keep active after changes have been made. This increases UX when doing multiple operations at a time
81131: Default location: Global — Default timerange: Relative — When opening an existing profile, save dialog will show current settings
81782: Shift book: Increased rights
82824: Shift book: Entries sorted by name
84288: Extension of the aggregation selection in the chart
84605: SwissKrono Customization SFTP Connection
Fixes¶
74101: Fixed an issue where the consumption of a counter was not displayed
76961: Export of the manual input works with special characters
77639: Fixed an issue where repeating values could not be saved
77912: Duplicating measurement points is also possible if the license is exceeded
78741: PROCON-WEB Connector in conjunction with value recording in case of value change leads to duplicate entries
79516: Fixed an issue where piecharts with absolute values in reports were not rendered correctly
79744: Fixed an issue where copying an empty cell did not completely clear fromer values from the clipboard
79769: Setpoint transfer cannot use decimal values
79821: Fixed an issue that could lead to duplicate shiftbook entries
80797: Changed pdf settings to avoid unnecessary save requests
81642: Deleting duplicate shift book entries leads to error according to the log
82007: Fixed error when “ “ in Medium / Ressourc
82038: Added an error page when a user logs in without user rights to display anything.
82239: Fixed an issue that could lead to export problems in combination with compatibility mode in a report
82428: Fixed an issue where an user could not be kicked
82557: Fixed an issue where multiple PROCON WEB connectors shared one queue swell. Each connector has its own swell
82744: Update a third party library that caused a freeze in live monitor pages when using gauges in specific constellations
82870: Quantity of rows displayed hand input v1 does not match configuration
84303: Pitfalls of licensing and duplicating measurement points
84653: No information to the user in case maximum payload is exceeded in communication over NATs during regression model creation and analysis
86913: Manual input: unnecessary number fields
87183: “Dokumente & Webanwendungen” didn´t work with Proxy anymore
87184: “Weblinks” didn´t work with Proxy anymore
87214: Auto export didn´t work with new login-page anymore
87360: ResMa tree, connector view: new advice can be created again
87363: ResMa tree, connector view: connector can be deleted
87528: Remove NX-Cache
88410: Report: Fixed calculating formula error with very small values
89237: Fixed saving profile with different timerange
89547: Same format for Timestamps in MQTT messages
89582: Dashboard profiles can be saved