ResMa 3.7.4

Release date: 2025-05-05

Service compatibility

This ResMa version is compatible with

  • Recipe Service v1.4.2

  • Import Service v1.1.3

  • Regression Service v1.0.3

Operating system compatibility

  • Windows 10 Pro

  • Windows 10 Enterprise

  • Windows 10 IoT Enterprise

  • Windows 11 Pro

  • Windows 11 Enterprise

  • Windows 11 IoT Enterprise

  • Windows Server 2016

  • Windows Server 2019

  • Windows Server 2022

  • Windows Server 2025

Features

  • 104000: Configuration of automatic data deletion based on time or size

  • 106345: IIoTConnector: Manual tag mapping when creating or changing a device

  • 106411: Revision and update of online help

  • 106518: Revision of derived quantities for alternative calculation

  • 102927: Database Backup Extension

  • 105890: User management: Description of permissions

  • 106179: Connector tag selection: Number of elements increased from 10 to 100

  • 106346: New dialog for manual connector tag mapping

  • 106400: Help for Repprt added for possible compression combinations

  • 106413: Release notes included in online help

  • 106648: Graphic objects in the report receive a manual adjustment of the X and Y alignment

  • 106649: Provide simple label as text field in LiveMonitor

  • 106983: IIoTConnector: no more automatic generation of measurement points

  • 107815: Improve import UI for old data import of the measurement point list

  • 107831: CO2 report updated

  • 108307: Certificate for HiveMQ is now generated via script

  • 109373: IIoTConnector: Write setpoints

Fixes

  • 74156: Strings via the ModbusConnector do not work

  • 88344: Chart: Chart starts with half a bar in monthly view

  • 88362: Chart: in the monthly view it is not clear which day is being viewed

  • 88364: Chart: after switching between year, month, week, day view, the Y-axis is not adjusted

  • 90783: Chart: Chart always shows one bar too many in bar display

  • 102183: Shift book: Icon present and refers to (deleted) shift book

  • 102185: Shift book: Icon for shift book cannot be moved

  • 102346: Report with order reference column remains empty for compression type counter difference

  • 102674: Manual input when “Display name” is deactivated, the field can no longer be moved

  • 103008: Tree is not updated for web link/shift book

  • 104057: Driver: The designer freezes during ResMa server import

  • 104361: Modbus Connector: Changing the slave ID in a connection does not update the config file

  • 104428: System info can no longer be downloaded

  • 104477: Modbus Connector remains permanently in “Reading Tag Value Failed” error after a timeout occurs during the first read

  • 104781: Report: Selection of order reference has no effect

  • 104846: Menu sometimes does not load when loading profile of a non-existent MicroService

  • 105438: Apostrophe in tag name causes problems with ResMa

  • 105939: MicroService pages do not load in automated Chrome in WebDriverIO

  • 106308: Report: Order reference “falsified” evaluation

  • 106393: Incorrect values ​​in time range without data

  • 106477: Login with smartphone not possible

  • 106834: CO2 report: Negative values ​​in report

  • 106950: CO2 report calculates incomprehensible values

  • 107105: Tag selection field too short during data import

  • 107210: Problems transferring the TagCache via NATS to ProconConnect

  • 107214: Reports with multiple pages in portrait and landscape format are incorrectly exported to PDF

  • 108478: Master data stored size cannot always be opened

  • 108479: Master data stored size contains connector

  • 109088: Min/Max values ​​no longer allow the entry of decimal values

  • 109264: Transfer ResMa->NATS->MQTT: incorrect timestamp

  • 109455: Crash due to error in CHP forecast plug-in

  • 104428: System info can no longer be downloaded

  • 110420: Requesting new tags does not return an updated tag list

  • 110502: Update Telerik UI for ASP.NET AJAX => CVE-2025-3600

Known issues