ResMa 3.7.3

Release date: 2024-12-12

Service compatibility

This ResMa version is compatible with

  • Recipe Service v1.4.0

  • Import Service v1.1.3

  • Regression Service v1.0.3

Operating system compatibility

  • Windows 10 Pro

  • Windows 10 Enterprise

  • Windows 10 IoT Enterprise

  • Windows 11 Pro

  • Windows 11 Enterprise

  • Windows 11 IoT Enterprise

  • Windows Server 2016

  • Windows Server 2019

  • Windows Server 2022

Features

  • 54799: Add warning when define counter with value change

  • 72839: Inform users about limited storage space on the installation partition

  • 72840: Inform users about almost full SQL Express database

  • 72841: Inform user about full message queue

  • 80364: Order of tabs within ResMa is saved

  • 81141: Profile name included in PDF export

  • 88502: Logging intervals of counters limited to reasonable ranges

  • 91416: Optionally add a resource to derived values

  • 91417: Price calculation for derived values in report

  • 91418: Price calculation for derived values in pivot

  • 91419: Price calculation for derived values in chart statistics

  • 95217: Introduction of an advanced mode for formulas of derived values

  • 95365: Update third party components with vulnerability issues

Fixes

  • 84912: Update value cache (Live Monitor) when value (e.g. string) is deleted

  • 85260: No measuring point monitor for manual input measuring points

  • 86263: Tab switching via menu referenced to the old position

  • 88363: Chart: Monthly view differed the sum of the daily value

  • 88711: Fixed measuring point list type selection

  • 88715: Scope in the C=2 can be inserted again

  • 88717: Resource column added as selection in measurement point list

  • 89953: Small Typo in automatic forwarding

  • 90029: Fixed time range selection in data import

  • 92263: Min/Max für abgeleitete Größe im Report wird falsch berechnet

  • 92631: Fixed display of end time in data import

  • 93040: Fixed deleting of auto exports with empty name in auto export view

  • 93571: Fixed error with deleted parameters in report

  • 94007: Do not delete used units

  • 94213: Fixed truncated or shifted content in PDF export

  • 94607: Fixed using of special characters in UI

  • 95564: Used units can be deleted - View of used objects

  • 95939: Error when loading time series

  • 95966: Manual input: Check value of numeric input

  • 96128: Manual input: Cut-out value again is displayed again

  • 96257: Manual input: Cut-out value will be saved as well

  • 96673: Fixed using of parameter %Aktuelle Werte% when sending alert mails

  • 97926: Manual input: Fixed display of dropdown list in options

  • 97653: Uninstall “Caddy ReverseProxy” when uninstall ResMa

  • 98028: Time series: Create new profile is now possible for a specific user

  • 98454: Deleting of profiles with long names in burger menu

  • 98457: “Wert kopieren auf” is written in PROCON-WEB ResMa Connector Log

  • 99433: User with global profiles transfers his global profiles when deleted

  • 9762: Manual trigger for requesting a tag list”

  • 99766: Creating a derived value with alias “A..” leads to an error

  • 99781: Fixed copy of formula in report when colum id >= AA

  • 101022: Fixed value change of boolean measuring point in value grid

  • 101075: Fixed display of profiles in burger menue after rename

  • 101256: Creating measurement point of PROCON Connect without a ressource works now

  • 101630: Fixed unit error in the modbus template for Janitza Prodata

  • 102193: Aligning time functions in StoredProcedures

Known issues

  • If the SlaveId of a DirectConnect connection is changed, this change is not immediately transferred to the connector. Therefore, a manual transfer via “Send configuration” is required afterwards