ResMa 3.8.0

Release date: 2025-10-15

Service compatibility

This ResMa version is compatible with

  • Recipe Management v1.4.3

  • Import Service v1.1.4

  • Regression Analysis v2.1.0

Operating system compatibility

  • Windows 10 Pro

  • Windows 10 Enterprise

  • Windows 10 IoT Enterprise

  • Windows 11 Pro

  • Windows 11 Enterprise

  • Windows 11 IoT Enterprise

  • Windows Server 2016

  • Windows Server 2019

  • Windows Server 2022

  • Windows Server 2025

Features

  • 20958: PWEB connector: Adjust data import behavior

  • 89294: Front End: Software maintenance

  • 103609: ResMa accepts multiple files in event logs

  • 103625: Update of NuGet packages

  • 104897: Database backup strategy for microservices (Recipe Management)

  • 105296: Update and integrate manual

  • 107898: ProconConnect MQTT configuration (external cloud) - Launch from ResMa

  • 110160: Chart: Calculate standard deviation as aggregation type and provide it in the chart

  • 110162: Manual input: Number of decimal places adjustable

  • 110163: Manual input: Link to report as from report to manual input

  • 110164: Manual input: Improved separation/spacing between the “Save” and “Timepicker” buttons

  • 110165: Manual input: Configure and integrate PLC values as read-only fields

  • 110168: Manual input: The same input fields can be configured and integrated multiple times

  • 110170: Manual input: Units can be hidden

  • 110205: Manual input: Update of the “Date Timepicker” after saving

  • 110206: Manual input: TimePicker (time entries) should only have minute precision at this point

  • 110209: Manual input: Notification to the user when saving if the time range is too far in the past

  • 110210: Manual input: Dropdown/input field should have configuration to align text left or right

  • 110214: Report: Report for the lab team in which several time series are displayed on a time grid in a table

  • 110215: Report: Report should also have the option for color selection

  • 110216: System: More granular permissions for profile and measurement point

  • 110217: Dashboard / Report: Refresh intervals too short and lead to poor usability

  • 110218: System: UUID (GUID) should be introduced in the master data “Measurement point”

  • 110219: System: In the asset tree, alarms are displayed between the symbol and the measurement point name

  • 110220: LiveMonitor: For each element, an option “Transparent background” can be activated.

  • 110355: Log user logins

  • 110580: Enhance error logs with more meaningful information

  • 110709: Update Caddy

  • 110710: Update HiveMQ and certificate

  • 110889: ResMa Combined SBOM

  • 110991: Resources validity period UX adjustment

  • 111087: More information about additional data

  • 111642: Adjustments of tag names similar to PWEB-Designer

  • 111661: Frontend: Update ResMa Shell UI to Angular 19

  • 111711: Searchable web directories

  • 111712: Webserver full path disclosure

  • 111713: TLS cookies without secure flag

  • 111714: Server version information disclosure

  • 112461: Email authentication with OAUTH2

  • 112614: Migration of email configuration page to Angular

  • 113591: Update jQuery

  • 114639: resma-shell-ui routing - breadcrumb handling

  • 115515: Revise ResMa texts

  • 116464: Links to user documentation in the Support Center for ResMa as well as for installed services are available in the GUI

Fixes

  • 88713: Conversion factor input mask not movable and incorrect decimal display

  • 101497: View on smartphone severely limited compared to older versions

  • 103696: NATS Timeout

  • 106910: Pivot view: Display of day, week and month leads to incorrect subdivision

  • 107410: Time series: Locked columns are not saved in profile

  • 109432: Setting up PROCON-WEB connector in ResMa only works after several attempts

  • 110083: Missing translations for fault forwarding

  • 110587: Translations cannot be deleted

  • 110820: ResMa password reset function has no effect

  • 111265: Additional information for MeMo communication (MQTT Input) raises questions from customers

  • 111399: ResMa creates “ghost connectors”

  • 112512: Determination of “AdditionalProperties” takes too long

  • 112563: Deleting individual values leads to automatic logout from ResMa

  • 112872: Derived metrics allow value input after a display change

  • 112934: Errors due to new properties in web.config

  • 112989: ResMa Driver Tag Template EM750 Impulse Input1-3 incorrect data type

  • 113271: Setup 6.10: ResMaConnectorService log file is not stored under C:PROCON-WEBLogs

  • 113398: When deleting a single resource, all resources are removed

  • 113424: Missing reference of a measurement parameter in the resource tree of ResMa

  • 113605: Labels are no longer displayed or loaded

  • 113755: Report import creates existing measurement points again

  • 113855: Report: The text field of the time display cannot be edited

  • 114382: Report: The input field cannot be edited

  • 114475: Report: In editing mode, no PDF file can be exported.

  • 114561: Dashboard refresh interval unit

  • 114810: LiveMonitor: no more measurement points can be added

  • 114854: When recreating the activation code for IoT connectors in ResMa, the newly created activation code is not saved

  • 115170: Incorrect text in LiveMonitor

  • 115525: Import of languages leads to error message

  • 115918: Profiles can no longer be saved as “Global”

  • 116054: Dashboard mode does not hide title

  • 116065: Labeling errors in the interface

  • 116122: Report: TypeError in console when clicking on cell in the table

  • 116124: Report: The data in the formula field appears in reverse order.

  • 116182: DataViewService: Chart CSV export does not work

  • 116279: Backend libraries cannot be displayed

  • 116280: Frontend library of regression analysis cannot be displayed

  • 116579: New LiveMonitor not functional

  • 116784: Selection of colors in the diagram is faulty

  • 116954: SPC chart and limit value analysis profile does not appear in the overview after saving