PROCON-WEB Embedded Systems 6.11.3¶
Warning
The system can therefore be accessed at https://localhost:17443.
Access via the old port is no longer possible.
Fixes & Improvements¶
129970: Fixed an issue that prevented alarms from being reset after a power loss and a restart of the host system.
Known issues¶
Firmware bug in Siemens 1500 CPUs with firmware 4.0: Frequent connection and disconnection with the PLC visible in the event log. Fix via firmware update from v4.0.4 brings improvement, but does not completely resolve the issue. Further information can be found in the Siemens Release Notes. TIA drivers are therefore not currently approved for firmware v4.x.
The setup for Windows systems does not configure port forwarding, so streaming does not work. On Windows, port 17443 must be manually opened in the Windows Defender Firewall under the inbound rules.