PROCON-WEB Embedded Systems 6.9.0

Features

  • 86161: Improved, revised navigation options, UIs and user flows.

  • 16546: Logbook for interactive entries.

  • 86802: X/Y chart for HMI WebRuntime.

  • 87727: REST APIs allow access to system functionality. Documentation of the interfaces in Open API format.

  • 84797: System variables can be managed in a separate tab in the tag overview.

  • 74548: OPC-UA driver can read structure-based and display structures in the client.

  • 94197: An export function has been added to the data logger and recipes.

Fixes

  • An issue has been fixed that caused write attempts of non-tag values to be called via the Tag API.

Known issues

  • If a tag for a driver is imported via the telemetry UI, it does not automatically appear in the tag list. The page must be refreshed, e.g. by pressing F5. Only occurs on u-OS, installations/deployments under Windows and Linux are not affected.