PROCON-WEB Embedded Systems 6.11.1

Warning

The port for accessing PROCON-WEB Embedded Systems has changed. The new port is now 17443.
The system now communicates securely, i.e. via HTTPS instead of HTTP.

The system can therefore be accessed at https://localhost:17443.

Access via the old port is no longer possible.

Fixes & improvements

  • 125201: A problem has been fixed that prevented offline licensing via the web UI. On Windows, the WIBU toolchain can be used for licensing as a workaround. Linux-based systems must update to v1.3.2 or license online.

Known issues

  • Firmware bug in Siemens 1500 CPUs with firmware 4.0: Frequent connection and disconnection with the PLC visible in the event log. Fix via firmware update from v4.0.4 brings improvement, but does not completely resolve the issue. Further information can be found in the Siemens Release Notes. TIA drivers are therefore not currently approved for firmware v4.x.

  • The TIA V2 driver does not currently support importing fields from structures. Instead, the driver creates an element for each index.

  • The setup for Windows systems does not create a port share, which is why streaming does not work. Port 17443 must be manually enabled in the Windows Defender Firewall in the incoming rules under Windows.