PROCON-Connect 1.0.3¶
Features¶
Improved, revised navigation options, UIs and user flows.
REST APIs allow access to system functionality. Documentation of the interfaces in Open API format.
OPC-UA driver can read structure-based and display structures in the client.
The MQTT client of the IIoT Connector now supports MQTT v3.1.1 in addition to MQTT v5.
Data loggers have been expanded to include an export function.
Fixes¶
Fixed an issue that caused the tag overview not to be updated automatically after a tag import.
Fixed an issue that prevented ResMa® from communicating with the NATS broker of PROCON-Connect.
Fixed an issue that caused write attempts of non-tag values to be called via the Tag API.
Fixed an issue that caused the IIoT Connector service to exit after reconnection attempts to an MQTT broker were unsuccessful for several hours.
Known issues¶
If a tag for a driver is imported via the telemetry UI, it does not automatically appear in the tag list. The page must be refreshed, e.g. by pressing F5. Only occurs on u-OS, installations/deployments under Windows and Linux are not affected.