PROCON-Connect 1.2.2¶
Fixes & Improvements¶
116247: Fixed an issue that caused the TIA v2 driver logging to fail to output all messages.
121037: Fixed an issue that caused the TIA v2 driver to write WStrings incorrectly.
115648: Fixed an issue that caused the TIA v2 driver to create empty structures when importing structures with HMI not visible variables.
119918: Fixed an issue that caused char arrays to not import correctly.
119615: Various minor adjustments, fixes, and improvements.
Known Issues¶
If a tag for a driver is imported via the telemetry UI, it does not automatically appear in the tag list. The page must be refreshed, e.g. by pressing F5. Only occurs on u-OS, installations/deployments under Windows and Linux are not affected.
Firmware bug in Siemens 1500 CPUs with firmware 4.0: Frequent connection and disconnection with the PLC visible in the event log. Fix via firmware update from v4.0.4 brings improvement, but does not completely resolve the issue. Further information can be found in the Siemens Release Notes. TIA drivers are therefore not currently approved for firmware v4.x.
The TIA V2 driver does not currently support importing fields from structures. Instead, the driver creates an element for each index.