PROCON-Connect 1.3.2¶
Warning
The system can be accessed at https://localhost:18443.
Access via http://localhost:16701 is no longer possible.
Fixes & improvements¶
125201: A problem has been fixed that prevented offline licensing via the web UI. On Windows, the WIBU toolchain can be used for licensing as a workaround. Linux-based systems must update to v1.3.2 or license online.
Known issues¶
If a tag for a driver is imported via the telemetry UI, it does not automatically appear in the tag list. The page must be refreshed, e.g. by pressing F5. Only occurs on u-OS, installations/deployments under Windows and Linux are not affected.
Firmware bug in Siemens 1500 CPUs with firmware 4.0: Frequent connection and disconnection with the PLC visible in the event log. Fix via firmware update from v4.0.4 brings improvement, but does not completely resolve the issue. Further information can be found in the Siemens Release Notes. TIA drivers are therefore not currently approved for firmware v4.x.
The TIA V2 driver does not currently support importing fields from structures. Instead, the driver creates an element for each index.