PROCON-Connect 1.2.1¶
Fixes¶
118758: Fixed an issue that prevented license tickets with multiple licenses from being automatically activated if some of the licenses had already been used previously.
117780: Fixed an issue that caused the runtime to crash due to a specific constellation in client scripting (only affects use in PROCON-WEB).
116247: Fixed an issue that caused the TIA driver’s event logging to not function correctly at the Trace log level.
118437: Fixed an issue that caused the tag count for licensing in HMI projects to be used incorrectly (only affects use in PROCON-WEB).
Known issues¶
If a tag for a driver is imported via the telemetry UI, it does not automatically appear in the tag list. The page must be refreshed, e.g. by pressing F5. Only occurs on u-OS, installations/deployments under Windows and Linux are not affected.