PROCON-Connect 1.2.0¶
Features¶
104984: PROCON-Connect can couple with the u-OS Datahub and exchange tags. Details under u-OS Datahub.
111800: SQLite data loggers can now also be created in-memory in addition to a file-based database. Details under Choosing the right database type.
111803: The deletion cycles for data loggers can now also be configured on a minute basis.
112537: The size of an SQLite database is now displayed in the Datalogger overview.
111819: Multiple SQLite databases can now be created. The file path to the database is now also configurable and can also be located on a USB device or an SD card. Details under SQLite file based.
104424: When opening the UI in an unlicensed state, a notification is displayed that can be used to activate demo mode directly. Details under Licensing.
110964: The OPC UA driver can now be configured for each connection whether tags in status uncertain should be treated as status good. This allows writing to tags in status uncertain.
110463: The visibility of the buttons in the connector overview and data logger overview has been improved.
Fixes¶
109047: Fixed an issue that caused the licensing of an InfluxDB link to only work after a restart.
109052: Fixed an issue that caused not all configuration changes to be saved when customizing an InfluxDB link.
106807: Fixed an issue that meant that it was no longer possible to switch projects via the project management UI.
110986: Fixed an issue that caused the interpolation to be performed incorrectly for a request over several tags of a data logger.
108806: Fixed an issue that caused the Codesys driver to ignore the static kill configuration.
108539: Fixed an issue that caused the OPC UA driver to not read structures in an optimized way.
108982: Fixed an issue that caused the OPC UA driver to import strings with the wrong length.
111629: Fixed an issue that caused connected cloud connectors to no longer display their status in the connector overview.
111200: Fixed an issue that caused license containers not to be created correctly.
110334: Fixed an issue that prevented connectors from being connected or disconnected across all UI elements.
110727: Fixed an issue that caused an error message to be displayed when connecting to an MQTT broker with an untrusted certificate.
110624: Fixed an issue that caused the number of messages for connections to Azure IoT Hub to be displayed incorrectly in the connector overview.
108263: Fixed an issue that caused the OPC UA driver to not correctly support multiple kill variables per connection.
112501: Fixed an issue that caused the driver status to be displayed incorrectly after stopping a driver service.
112503: Fixed an issue that caused the Allen-Bradley driver to not read all tags after a restart.
Known issues¶
If a tag for a driver is imported via the telemetry UI, it does not automatically appear in the tag list. The page must be refreshed, e.g. by pressing F5. Only occurs on u-OS, installations/deployments under Windows and Linux are not affected.