File management¶
General¶
In the PROCON-WEB Designer it is possible to manage external files.
Typical files are, for example, the “external.css”, which can also adapt the runtime interface, and the “external.js”, in which, among other things, custom controls can be defined.
Surface¶
The file management surface is a typical grid in the PROCON-WEB Designer
The name is determined by the name of the selected file and cannot be changed. In addition, a description can be created for each file.
The additional parameters “Export” and “Target” determine whether the file should be copied with the project export and to which location (project or WebVisu directory).
Important
If a file with the same name is used or exported several times, the existing file will be overwritten.
Important
The order in the file management schedules the order in which the files will be exported resp. processed .