Special functions¶
Special functions in a summary¶
Special functions can be triggered from the event code via symbols, texts and function keys. Special functions are successively replaced by self-explanatory function calls. Special functions are also not fully available for all server variants!To start a certain special function, the corresponding special function number must be assigned as a parameter or selected via the special function selection
Available special functions¶
ID |
Descritpion |
|---|---|
203 |
Log in user |
204 |
Change user passwort |
205 |
Log out user |
206 |
Call up the user administration |
207 |
TokenLoginDialog |
413 |
Restart the user interface |
420 |
Show help buttons |
422 |
Show all tooltips |
423 |
Hide all tooltips |
430 |
Show information window |
431 |
Call up the device assignment dialog |
1253 |
Call up the dialog to switch the language |
6xxx |
Call up picture xxx as an additional dialog |
6999 |
Close current dialog |
7xxx |
Change to picture xxx |
Special functions - selection¶
This selection window can be opened with the right mouse button at all points in the Designer where special functions must be entered or specified. A special function is selected with a mouse click and the selection is accepted with the ‘OK’ button.